| 
    Legrand / Raritan / Server Technology Xerus™ JSON-RPC API
    
   | 
 
Peripheral Devices. More...
Classes | |
| struct | Address | 
| peripheral device position based address  More... | |
| interface | BatteryPoweredDevicePackage | 
| struct | Device | 
| A peripheral device is the collection of.  More... | |
| struct | DeviceID | 
| peripheral device identification  More... | |
| interface | DeviceManager | 
| Peripheral Device Manager.  More... | |
| interface | DeviceSlot | 
| Peripheral Device Slot.  More... | |
| interface | DoorHandleControllerPackage | 
| interface | G2Production | 
| interface | GatewaySensorManager | 
| Gateway Sensor Configuration Interface.  More... | |
| interface | ModbusCfg | 
| interface | Package | 
| struct | PackageInfo | 
| Peripheral device package information.  More... | |
| struct | PosElement | 
| peripheral device position element, list forms position  More... | |
| interface | SensorHub | 
| Sensor Hub interface.  More... | |
Enumerations | |
| enum | PortType {  ONBOARD , DEV_PORT , ONEWIRE_HUB_PORT , ONEWIRE_CHAIN_POS , REMOTE_HUB_PORT , WIRELESS_BRIDGE , WIRELESS_DEVICE , UNSPECIFIED , GATEWAY_SENSOR , FEATURE_PORT , USB_PORT , USB_HUB_PORT , USB_RS485_DONGLE }  | 
| peripheral device port types  More... | |
Peripheral Devices.
| enum peripheral::PortType | 
peripheral device port types
Definition at line 13 of file PosElement.idl.