Legrand / Raritan / Server Technology Xerus™ JSON-RPC API
|
Network Configuration. More...
Classes | |
struct | CommonInfo |
Common info. More... | |
struct | CommonInfoChangedEvent |
Event that is send when common network info has changed. More... | |
struct | CommonSettings |
Common settings. More... | |
interface | Diagnostics |
Diagnostics interface. More... | |
struct | DnsInfo |
DNS info. More... | |
struct | DnsSettings |
DNS settings. More... | |
struct | EapAuthSettings |
EAP authentication settings. More... | |
struct | EthInfo |
Ethernet interface info. More... | |
struct | EthInfoChangedEvent |
Event that is send when ethernet interface specific network info has changed. More... | |
struct | EthLinkMode |
Ethernet link mode. More... | |
struct | EthSettings |
Ethernet interface settings. More... | |
struct | Info |
Network info. More... | |
struct | InterfaceInfo |
Interface specific info. More... | |
struct | InterfaceInfoChangedEvent |
Event that is send when common interface specific network info has changed. More... | |
struct | InterfaceIpSettings |
Interface specific IP settings. More... | |
struct | InterfaceIPv4Info |
Interface specific IPv4 info. More... | |
struct | InterfaceIPv6Info |
Interface specific IPv6 info. More... | |
struct | InterfaceSettings |
Interface specific settings. More... | |
struct | IpAddrCidr |
IPv4/IPv6 address and prefix len. More... | |
struct | IpRoute |
IPv4/IPv6 route. More... | |
struct | IpRoutingSettings |
IP protocol specific routing settings. More... | |
struct | LinkStateChangedEvent |
Event that is send when the operational state of an interface changed. More... | |
interface | Net |
Network configuration interface. More... | |
struct | PortForwardingExpansionUnitPresenceStateChangedEvent |
Event that is send when the presence state of a downstream port forwarding expansion unit changes. More... | |
struct | PortForwardingInfo |
Port forwarding info. More... | |
struct | PortForwardingPrimaryUnitAddrInfo |
Port forwarding primary unit address info for an interface. More... | |
struct | PortForwardingProtocolMapping |
Mapping from application protocol id to name and transport protocol. More... | |
struct | PortForwardingSettings |
Port forwarding settings. More... | |
struct | RoutingInfo |
Routing info. More... | |
struct | RoutingSettings |
Routing settings. More... | |
interface | Services |
Network services configuration interface. More... | |
struct | ServiceSettings |
Network service settings. More... | |
struct | Settings |
Network settings. More... | |
struct | WlanInfo |
WLAN interface info. More... | |
struct | WlanInfoChangedEvent |
Event that is send when WLAN interface specific network info has changed. More... | |
struct | WlanSettings |
WLAN interface settings. More... | |
Enumerations | |
enum | PortForwardingRole { PRIMARY_UNIT , EXPANSION_UNIT } |
Role of the node when port forwarding is enabled. More... | |
enum | IpConfigMethod { STATIC , DHCP , AUTO } |
IP configuration method. More... | |
enum | InterfaceType { ETHERNET , WLAN , BRIDGE } |
The interface type. More... | |
enum | InterfaceOpState { NOT_PRESENT , DOWN , NO_LINK , UP } |
Interface operational state. More... | |
enum | EapOuterAuthMethod { EAP_PEAP , EAP_TLS } |
EAP outer authentication method. More... | |
enum | EapInnerAuthMethod { INNER_EAP_MSCHAPv2 , INNER_EAP_TLS } |
EAP inner authentication method. More... | |
enum | EapStatus { EAP_STATUS_DISABLED , EAP_STATUS_PENDING , EAP_STATUS_FAILED , EAP_STATUS_SUCCESS } |
EAP authentication status. More... | |
enum | EthSpeed { SPEED_AUTO , SPEED_MBIT_10 , SPEED_MBIT_100 , SPEED_MBIT_1000 } |
Ethernet speed. More... | |
enum | EthDuplexMode { DUPLEX_MODE_AUTO , DUPLEX_MODE_HALF , DUPLEX_MODE_FULL } |
Ethernet duplex mode. More... | |
enum | EthAuthType { ETH_AUTH_NONE , ETH_AUTH_EAP } |
Ethernet authentication type. More... | |
enum | WlanSecProtocol { WPA2 } |
WLAN security protocol. More... | |
enum | WlanAuthType { WLAN_AUTH_NONE , WLAN_AUTH_PSK , WLAN_AUTH_EAP } |
WLAN authentication type. More... | |
enum | WlanChannelWidth { CHANNEL_WIDTH_UNKNOWN , CHANNEL_WIDTH_20_NO_HT , CHANNEL_WIDTH_20 , CHANNEL_WIDTH_40 , CHANNEL_WIDTH_80 , CHANNEL_WIDTH_80P80 , CHANNEL_WIDTH_160 } |
WLAN channel width. | |
Network Configuration.
Network services configuration.
enum net::EapStatus |
enum net::EthAuthType |
enum net::EthDuplexMode |
enum net::EthSpeed |
enum net::InterfaceType |
enum net::IpConfigMethod |
enum net::WlanAuthType |
enum net::WlanSecProtocol |