Legrand / Raritan / Server Technology Xerus™ PDU JSON-RPC API
|
User Management More...
Classes | |
struct | Account |
Account information More... | |
struct | AccountAdded |
This event is emitted after a new account with the provided username was added. More... | |
struct | AccountChanged |
This event is emitted if the settings of an account as defined in usermgmt::UserInfo have changed (Note: we may add an indication what in the structure has changed or even split the event, if handling is difficult) More... | |
struct | AccountEvent |
Base type of all account event. More... | |
struct | AccountRemoved |
This event is emitted after the account with the provided username has been removed. More... | |
struct | AccountRenamed |
This event is emitted after an account has been renamed. More... | |
struct | AuxInfo |
Auxiliary user information. More... | |
struct | PasswordChanged |
This event is emitted after the password for an account was changed. More... | |
struct | Preferences |
User preferences More... | |
interface | Role |
Role management interface More... | |
struct | RoleAdded |
struct | RoleChanged |
struct | RoleEvent |
Base type of all account event. More... | |
interface | RoleManager |
Role manager interface. More... | |
struct | RoleRemoved |
struct | SnmpV3Settings |
SNMPv3 settings. More... | |
interface | User |
User interface More... | |
struct | UserCapabilities |
User Capabilities Describe if certain operations can be performed for user. More... | |
struct | UserInfo |
User information More... | |
interface | UserManager |
User manager interface More... | |
Enumerations | |
enum | SnmpV3SecLevel { NO_AUTH_NO_PRIV , AUTH_NO_PRIV , AUTH_PRIV } |
SNMPv3 security level. More... | |
enum | SnmpV3AuthProto { MD5 , SHA1 , SHA224 , SHA256 , SHA384 , SHA512 } |
SNMPv3 authentication protocol. More... | |
enum | SnmpV3PrivProto { DES , AES128 , AES192 , AES256 , AES192_3DES , AES256_3DES } |
SNMPv3 privacy protocol. More... | |
enum | TemperatureEnum { DEG_C , DEG_F } |
Preferred display unit for temperature sensors. More... | |
enum | LengthEnum { METER , FEET } |
Preferred display unit for length measurements, e.g. More... | |
enum | PressureEnum { PASCAL , PSI } |
Preferred display unit for (air) pressure sensors. More... | |
User Management
enum usermgmt::LengthEnum |
SNMPv3 authentication protocol.
SNMPv3 privacy protocol.