Legrand / Raritan / Server Technology Xerus™ PDU JSON-RPC API
|
PDU Model. More...
Classes | |
interface | Ade |
Interface for ADE chips directly connected to main controller. More... | |
interface | Circuit |
BCM circuit. More... | |
struct | CircuitBreakerStatistic |
Overcurrent protector statistics. More... | |
interface | Controller |
Sub controller interface. More... | |
struct | CtrlStatistic |
Sub controller statistics. More... | |
struct | DoublePole |
for OCP More... | |
interface | EDevice |
Common base interface for any kind of electrical device that is used in the PDU model, such as inlets, OCPs and outlets. More... | |
interface | Inlet |
Inlet interface More... | |
interface | MemoryMapController |
Memory map controller. More... | |
struct | MeteredLinePair |
An inlet line pair. More... | |
struct | Nameplate |
Component nameplate information. More... | |
interface | Outlet |
Outlet interface More... | |
interface | OutletGroup |
Outlet group interface. More... | |
interface | OutletGroupManager |
Outlet group manager interface. More... | |
struct | OutletStatistic |
Outlet statistics More... | |
interface | OverCurrentProtector |
Overcurrent protector interface. More... | |
interface | OverCurrentProtectorTripSensor |
Overcurrent protector trip sensor interface. More... | |
interface | Panel |
PMC panel. More... | |
interface | Pdu |
Main PDU interface. More... | |
struct | Pole |
An inlet or outlet pole. More... | |
interface | PowerMeter |
A three-phase power meter (PMC). More... | |
interface | PowerMeterController |
Power Meter Controller (PMC) interface. More... | |
interface | PowerQualitySensor |
Power quality sensor interface. More... | |
struct | Rating |
Numerical usage ratings. More... | |
interface | ResidualCurrentStateSensor |
Residual current state sensor interface. More... | |
struct | ThrowPole |
A pole that can select one of multiple inputs. More... | |
interface | TransferSwitch |
Transfer switch interface. More... | |
interface | TypeBResidualCurrentNumericSensor |
An RCM current sensor of type B (AC/DC) which allows degaussing the sensor. More... | |
interface | Unit |
Unit interface. More... | |
interface | VoltageMonitoringSensor |
Interface of a voltage sensor with extended monitoring capabilities. More... | |
struct | Waveform |
Waveform data, including metadata. More... | |
Enumerations | |
enum | PowerLine { L1 , L2 , L3 , NEUTRAL , EARTH , PLUS , MINUS } |
Power line. More... | |
PDU Model.
enum pdumodel::PowerLine |