| 
    Raritan / Server Technology Xerus™ PDU JSON-RPC API
    
   | 
 
PDU Model. More...
Classes | |
| interface | Ade | 
| Interface for ADE chips directly connected to main controller.  More... | |
| interface | Circuit | 
| BCM circuit.  More... | |
| struct | CtrlStatistic | 
| Sub controller statistics.  More... | |
| interface | Controller | 
| Sub controller interface.  More... | |
| interface | EDevice | 
| Common base interface for any kind of electrical device that is used in the PDU model, such as inlets, OCPs and outlets.  More... | |
| interface | Inlet | 
| Inlet interface  More... | |
| interface | MemoryMapController | 
| Memory map controller.  More... | |
| struct | Rating | 
| Numerical usage ratings.  More... | |
| struct | Nameplate | 
| Component nameplate information.  More... | |
| struct | OutletStatistic | 
| Outlet statistics  More... | |
| interface | Outlet | 
| Outlet interface  More... | |
| interface | OutletGroup | 
| Outlet group interface.  More... | |
| interface | OutletGroupManager | 
| Outlet group manager interface.  More... | |
| struct | CircuitBreakerStatistic | 
| Overcurrent protector statistics.  More... | |
| interface | OverCurrentProtector | 
| Overcurrent protector interface.  More... | |
| interface | OverCurrentProtectorTripSensor | 
| Overcurrent protector trip sensor interface.  More... | |
| interface | Panel | 
| PMC panel.  More... | |
| interface | Pdu | 
| Main PDU interface.  More... | |
| struct | Pole | 
| An inlet or outlet pole.  More... | |
| struct | MeteredLinePair | 
| An inlet line pair.  More... | |
| struct | DoublePole | 
| for OCP  More... | |
| struct | ThrowPole | 
| A pole that can select one of multiple inputs.  More... | |
| interface | PowerMeter | 
| A three-phase power meter (PMC).  More... | |
| interface | PowerMeterController | 
| Power Meter Controller (PMC) interface.  More... | |
| interface | PowerQualitySensor | 
| Power quality sensor interface.  More... | |
| interface | ResidualCurrentStateSensor | 
| Residual current state sensor interface.  More... | |
| interface | TransferSwitch | 
| Transfer switch interface.  More... | |
| interface | TypeBResidualCurrentNumericSensor | 
| An RCM current sensor of type B (AC/DC) which allows degaussing the sensor.  More... | |
| interface | Unit | 
| Unit interface.  More... | |
| interface | VoltageMonitoringSensor | 
| Interface of a voltage sensor with extended monitoring capabilities.  More... | |
| struct | Waveform | 
| Waveform data, including metadata.  More... | |
Enumerations | |
| enum | PowerLine {  L1 , L2 , L3 , NEUTRAL , EARTH , PLUS , MINUS }  | 
| Power line.  More... | |
PDU Model.
| enum pdumodel::PowerLine |