Legrand / Raritan / Server Technology Xerus™ JSON-RPC API
Loading...
Searching...
No Matches
peripheral Module Reference

Peripheral Devices. More...

Classes

struct  Address
 peripheral device position based address More...
interface  BatteryPoweredDevicePackage
struct  Device
 A peripheral device is the collection of. More...
struct  DeviceID
 peripheral device identification More...
interface  DeviceManager
 Peripheral Device Manager. More...
interface  DeviceSlot
 Peripheral Device Slot. More...
interface  DoorHandleControllerPackage
interface  G2Production
interface  GatewaySensorManager
 Gateway Sensor Configuration Interface. More...
interface  ModbusCfg
interface  Package
struct  PackageInfo
 Peripheral device package information. More...
struct  PosElement
 peripheral device position element, list forms position More...
interface  SensorHub
 Sensor Hub interface. More...

Enumerations

enum  PortType {
  ONBOARD , DEV_PORT , ONEWIRE_HUB_PORT , ONEWIRE_CHAIN_POS ,
  REMOTE_HUB_PORT , WIRELESS_BRIDGE , WIRELESS_DEVICE , UNSPECIFIED ,
  GATEWAY_SENSOR , FEATURE_PORT , USB_PORT , USB_HUB_PORT ,
  USB_RS485_DONGLE
}
 peripheral device port types More...

Detailed Description

Peripheral Devices.

Enumeration Type Documentation

◆ PortType

peripheral device port types

Enumerator
ONBOARD 

a built in, inaccessible port

DEV_PORT 

a sensor port on the device

ONEWIRE_HUB_PORT 

a port on a Hub

ONEWIRE_CHAIN_POS 

a chain position

REMOTE_HUB_PORT 

a RS485 remote hub port

WIRELESS_BRIDGE 

a wireless bridge, e.g. usb dongle

WIRELESS_DEVICE 

a wireless device

UNSPECIFIED 

device type is unknown

GATEWAY_SENSOR 

a gateway sensor

FEATURE_PORT 

the feature port

USB_PORT 

USB port.

USB_HUB_PORT 

USB hub port.

USB_RS485_DONGLE 

USB dongle with rs485 port.

Definition at line 13 of file PosElement.idl.