Legrand / Raritan / Server Technology Xerus™ JSON-RPC API
Loading...
Searching...
No Matches
Classes | Enumerations
pdumodel Module Reference

PDU Model. More...

Classes

interface  Circuit
 BCM circuit. More...
 
struct  CircuitBreakerStatistic
 Overcurrent protector statistics. More...
 
interface  Controller
 Sub controller interface. More...
 
struct  CtrlStatistic
 Sub controller statistics. More...
 
struct  DoublePole
 for OCP More...
 
interface  EDevice
 Common base interface for any kind of electrical device that is used in the PDU model, such as inlets, OCPs and outlets. More...
 
interface  Inlet
 Inlet interface More...
 
interface  MemoryMapController
 Memory map controller. More...
 
struct  MeteredLinePair
 An inlet line pair. More...
 
struct  Nameplate
 Component nameplate information. More...
 
interface  Outlet
 Outlet interface More...
 
interface  OutletGroup
 Outlet group interface. More...
 
interface  OutletGroupManager
 Outlet group manager interface. More...
 
struct  OutletStatistic
 Outlet statistics More...
 
interface  OverCurrentProtector
 Overcurrent protector interface. More...
 
interface  OverCurrentProtectorTripSensor
 Overcurrent protector trip sensor interface. More...
 
interface  Panel
 PMC panel. More...
 
interface  Pdu
 Main PDU interface. More...
 
struct  Pole
 An inlet or outlet pole. More...
 
interface  PowerMeter
 A three-phase power meter (PMC). More...
 
interface  PowerMeterController
 Power Meter Controller (PMC) interface. More...
 
interface  PowerQualitySensor
 Power quality sensor interface. More...
 
struct  Rating
 Numerical usage ratings. More...
 
interface  ResidualCurrentStateSensor
 Residual current state sensor interface. More...
 
struct  ThrowPole
 A pole that can select one of multiple inputs. More...
 
interface  TransferSwitch
 Transfer switch interface. More...
 
interface  TransferSwitchBypassStateSensor
 Overcurrent protector trip sensor interface. More...
 
interface  TypeBResidualCurrentNumericSensor
 An RCM current sensor of type B (AC/DC) which allows degaussing the sensor. More...
 
interface  Unit
 Unit interface. More...
 
interface  VoltageMonitoringSensor
 Interface of a voltage sensor with extended monitoring capabilities. More...
 
struct  Waveform
 Waveform data, including metadata. More...
 

Enumerations

enum  PowerLine {
  L1 , L2 , L3 , NEUTRAL ,
  EARTH , PLUS , MINUS
}
 Power line. More...
 

Detailed Description

PDU Model.

Enumeration Type Documentation

◆ PowerLine

Power line.

Enumerator
L1 

Line 1.

L2 

Line 2.

L3 

Line 3.

NEUTRAL 

Neutral.

EARTH 

Earth.

PLUS 

Positive (DC)

MINUS 

Negative (DC)

Definition at line 18 of file Pole.idl.